6/24/2007 1:31 PM | |
Posts: 75 Rating:
|
But in manual https://support.automation.siemens.com/WW/llisapi.dll/8676999?nodeid0=10806053&func=ll&objId=8676999&objAction=csView&caller=view&lang=en&siteid=cseus&aktprim=0&extranet=standard&load=content 3.3 Redundant Coupling of Network Segments The standby-sync port of an OSM/ESM with 8 ports allows the connection of two Industrial Ethernet OSMs or ESMs with one operating as standby master (DIP switch "Stby off") and the other as standby slave (DIP switch "Stby on"). With this mode, pairs of OSMs/ESMs can be used for redundant coupling of OSM/ESM or OLM rings. With network management, the OSM/ESM can also be configured so that several rings or networks can be interconnected at the same time with two OSMs/ESMs (see OSM/ESM Network Management, User Manual /1/). |
Follow us on