Industry Online Support
Technical Forum
4/18/2007 9:12 AM | |
Posts: 1084 Rating: (72)
|
hi, If you have two pc's both with wincc installed (ensure that you install the redundancy option aswell, you can select it during normal install as an option); you can create one wincc server project. You can setup redundancy as an option within the project after which you can duplicate the project to the other pc. That's basically it. Please refer to the wincc information center after install for further details. It depends on which version of wincc you are going to use to determine the OS you need. Search for the compatibility list to be able to determine this. with regards, Ikkezelf |
4/18/2007 1:34 PM | |
Posts: 1275 Rating: (123)
|
Hi, You should, as Ikkezelf said, always check compatibility between WinCC, the OS (for servers and clients) and other Siemens software. For OS server compatibility there's this attachment. Best regards, Danielle AttachmentWinCC_Windows_Serverkompatibilitaeten_e.pdf (130 Downloads) |
Follow us on