5/27/2025 3:22 AM | |
Joined: 12/18/2014 Last visit: 9/16/2025 Posts: 35965 Rating:
|
Redundant IO modules connected to SIMATIC S7-1500Application example: IO modules can have a redundant connection to a SIMATIC S7-1500 and can be monitored If the availability of sensor and/or actuator loops needs to be enhanced, this application offers effective solutions. By incorporating redundancy of the IO-modules connected to single or redundant sensors/actuators, the availability of these loops will be significantly improved. Thanks to the monitoring performed by the "LRedIo" function blocks, even in the event of an IO-module or channel failure, the automation system will continue to operate, ensuring that the customer process remains unaffected. |
This contribution was helpful to
1 thankful Users |
Follow us on