9/29/2013 2:33 PM | |
Posts: 4 Rating: (0) |
Hello, There are tricks u can use to make a base setting and then do some fine tuning. Best thing u can do (after configurating the FB41) is to put the controller in manual. After the temperature is stable. make a controller output change of 10% (if possible). Then record this in a trend with clear time indication. Now it is important that PV, SP, LMN are fed to the controller as percents (0-100%). So, if the temperature is 0-400°C you have to convert it to 0-100%,. Note, it will work if you don't, but if you want to calculate your base setting, then 0-100% range is neccesary. Now if you have a PT100 input then just chose a valid range and convert this range from 0-100%. Now you can put the times in the attached excel. This will not always work, but for me its always close. And the last tip i can give, is to understand PID parameters. Good luck. AttachmentPID CalculatieEng.zip (306 Downloads) |
Last edited by: CS Moderator at: 10/14/2013 12:09 PMnew subject after splitting from /tf/WW/en/Posts/97898 |
|
This contribution was helpful to1 thankful Users |
9/29/2013 10:31 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello, Nice idea for providing tips for tuning based on process reaction curve. There are some points to discuss:
Best regards, Hamid Hosseini |
Last edited by: hdhosseini at: 10/1/2013 6:02 AMLast edited by: hdhosseini at: 9/29/2013 10:40 PM// New Link added |
|
This contribution was helpful to1 thankful Users |
10/2/2013 4:41 AM | |
Posts: 209 Rating: (2) |
Hi autobot... Could you explain how to use this excel you gave?? It might be very helpful for me.. Thanks best regards raffy |
10/11/2013 7:47 AM | |
Posts: 7 Rating: (0) |
Thank you on your answer. Sometimes it seems impossible to make it perfect. |
This contribution was helpful to3 thankful Users |
Follow us on