9/9/2008 7:09 AM | |
Posts: 487 Rating: (36) |
Hi Another option ( maybe) is to use VPN and remote desktop to connect to a central PC at the workplace , this PC is then used to connect to the PLC's.Each user has is own user account ,if one leaves then delete account. To connect to customers it may be a bit more difficult .You use a call-back kind of system .You call the client via telephone and he switches on the modem or the internet connection. Speaking under correction you could use a scalance X .Have a look at the this link there is a lot of info on connecting to PLC via networks Greetings Eric |
9/9/2008 8:22 AM | |
Joined: 3/21/2006 Last visit: 11/1/2024 Posts: 10229 Rating: (1181) |
Hi Eric At the moment I use this type of connection. With Remote desktop (RealVNC) with PC in office we can connect to each PLC, of course together with VPN. Dissadvantages - must install all software + license . . Maybe better is to use VPN with SCALANCE s602. , yes of course need CP, connected to CPU. regards |
Follow us on