8/25/2015 10:36 PM | |
Posts: 111 Rating: (1) |
I am replacing siemens servo motor 1FK70423BK711RA0 WITH SIEMENS servo motor 1FK70423BK711RB0 the only reason to change this servo motor is to add brakes to remove the coast of motor as when somebody break the light curtain motor stop right away. I was just concerned do we have to do any programming changes as well by replacement of motor or it will work right away on the same parameters as of previous one and on the same encoder values as of the previous one or we have to re program encoder. Can anybody help. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/26/2015 11:15:09 AMNew subject after splitting |
|
Follow us on