8/27/2008 8:03 AM | |
Posts: 3 Rating: (0) |
Hi All, This Thread I am re-posting , as it has been closed -Apologise for the inconvienience caused .. SCADA system is unacceptably slow to operate and suffers from serious stability issues . The 2 SCADA Server System often fail to match up and will often lose communication with different areas of the plant for seemingly random intervals SCADA Machines Details :· Windows OS with Service Pack = Windows XP Professional Version 2002 Service Pack - 1· RAM =1 GB· Hard Drive Utilised Vs. Spare =C-Drive - 6.22GB / 9.98GB D-Drive - 9.15GB/101GB Software Versions Installed on SCADA machine :Simatic Net System architecture: In addition to other network ,Siemens 6 S7 PLC’s communicating on Ethernet network with the Rsview 32 via CP1613SCADA machine via lan Card over OPC Network Windows System and application log Errors: Please find attached herewith System Log Files and Application log Files for your ready reference Could you please have a glance on the System event message -1.bmp and System event message -2.bmp snapshots ,asthis error keep on coming all the time and slowing down and all the screens freezed out needs to reboot the machine . Thanks in advance. SVK Attachmentapplication Event Messages.zip (265 Downloads) |
8/27/2008 11:38 PM | |
Joined: 9/1/2005 Last visit: 1/17/2025 Posts: 4114 Rating: (195) |
closed cause question posted more than once. The thread where this question should be discussed is published with the subject Rsview 32 SCADA machine losing the comms with PLCs and slow down issue .Urgent. !!! within the conference Meet & Talk. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on