3/3/2016 5:00 PM | |
Posts: 5225 Rating:
|
Using as reference.. Information given in heading.. For your case - ----------------------------------------------------- There is nothing stopping you from using MC_MoveJog to control your axis for movement other than manual control. If you have a variable on the Velocity pin of the function - like on mine it is #CONTROL.MANUAL.SPEED - you could have complete control of your system. Making the movement works is now easy - but stopping accurately is a problem. ----------------------------------------------------- Using MC_Home the system can automatically hunt for the reference switch/sensor. If the reference switch is know, the system can work effectively with an absolute co-ordinate system. Automatically the movement will be forward if the target position is higher than the actual position and reverse if the target position is smaller than the actual position. Thereafter MC_MoveAbsolute can be used with confidence. ----------------------------------------------------- MC_MoveVelocity is a speed control without control of position... but you can read the position as mentioned above. Here the direction can be set by "Direction" pin of the function. To stop the motion you need to use MC_Halt. MC_Halt can also be used to abort MC_MoveAbsolute that is busy.. for example reaching a sensor position. For further review.... |
Last edited by: William_B at: 3/3/2016 5:22:36 PM |
|
3/3/2016 8:37 PM | |
Joined: 2/2/2016 Last visit: 2/1/2023 Posts: 220 Rating:
|
Thank you , I really appreciate your help. I will try it and tell you the results |
Follow us on