11/11/2011 10:11 AM | |
Joined: 8/16/2010 Last visit: 9/24/2024 Posts: 637 Rating: (12) |
Ok... But how to realize that in LAD. I never used Graph... |
11/17/2011 8:09 PM | |
Joined: 8/16/2010 Last visit: 9/24/2024 Posts: 637 Rating: (12) |
Hi all... I am done this...(attached pdf) But I thimk that there is better solution. What if system have 20 motors?! If someone have better solution. please post. Best regards AttachmentOB1.pdf (284 Downloads) |
12/3/2011 6:41 AM | |
Posts: 50 Rating: (6) |
Hi.Maybe you can use a (flip-flop) instuction to start-stop motor.That means one pulse set an output second pulse reset the output.And for the sequense an UP-DOWN counder,withc will increase or decrease from a pulse timer.After you have to give ID numbers to your motors acording to the sequence you wand to start.So every time the counder change value the motor with the same ID number will Start or stop
AttachmentSTART_STOP_MOTORS.zip (251 Downloads) |
Last edited by: glinglin at: 12/3/2011 12:38 PM |
|
12/6/2011 9:41 PM | |
Joined: 8/16/2010 Last visit: 9/24/2024 Posts: 637 Rating: (12) |
Thanks all. Glinglin I cannot open your solution. Whic version of TIA you use? huggy_d1 how to realize your solution, i dont understand? Little more help... |
12/7/2011 10:02 AM | |
Posts: 50 Rating: (6) |
I am using V11 SP1 UD2.But i have try to convert the project also to V10.5
AttachmentProject5.zip (233 Downloads) |
12/21/2015 1:59 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by Shahjee is split to a separate thread with the subject Ladder logic to start/stop motor using only one button. Best regards |
Follow us on