7/5/2010 3:30 PM | |
Posts: 5822 Rating: (411)
|
Dear mef3000, as far as I see it this should be possible. Changing this line topology to a redundant ring topology should work. The only point I can not verify right now is if the restrictionsfor the segment or the network size are being matched with your configuration. This would have to be verified with the manual for the PROFIBUS OLM to see if your network is useable. |
7/16/2010 12:26 PM | |
Posts: 5822 Rating: (411)
|
Hello, If you read the Manual: Operating Instructions SIMATIC NET PROFIBUS Optical Link Module OLM/P11 V4.0, OLM/P12 4.0, OLM/G11 V4.0, OLM/G12 V4.0, OLM/G12-EEC V4.0, OLM/G11-1300 V4.0, OLM/G12-1300 V4.0, you will find at page 22, in chapter 4.2.3.1 Setting the compatibility, that the OLM V 3 are fully compatible with the OLM V 4. Best regards J_Bell |
This contribution was helpful to1 thankful Users |
Follow us on