11/6/2017 4:55 PM | |
Joined: 10/11/2006 Last visit: 4/26/2024 Posts: 5825 Rating: (789)
|
Hello, for the functionality of cross cutting (rotary knife) or flying saw (linear knife axis) I can share the link to the applications for an S120 drive system. It is running directly inside the drive. On the PLC side you just set the commands (also therefore there are ready to use FBs for those drive applications). Here the links: https://support.industry.siemens.com/cs/de/en/view/109477746 (rotary knife) https://support.industry.siemens.com/cs/de/en/view/109477745 (flying saw) As I said for these applications you would need an S120 drive system. Of course also other solutions are available (SIMOTION, S7-1500T). For selecting the right drive size, motors etc. I would suggest to use the Sizer tool or to contact your local Siemens sales partner. He can help you to select the correct devices. This is the best solution I guess. |
With best regards, |
|
11/6/2017 7:36 PM | |
Posts: 2 Rating: (0) |
thanks for your response, my application is close to flying saw. |
Follow us on