10/20/2015 6:18 PM | |
Posts: 111 Rating: (1) |
I am using S110 (CU305 PM340) and I replace the motor 1FK70423BK711RA0 with 1FK70423BK711RB0 to add the brake to the motors but when I was commissioning it and change the parameter P1215 = 1 and try to move the motor it was not releasing the brakes can anybody tell me what could be the problem? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/21/2015 12:02:29 PMNew subject after splitting |
|
10/21/2015 1:10 PM | |
Posts: 111 Rating: (1) |
Yes I did. I use relay 24VDC Omron Relay and actuate the coil of the brake with terminals on PM340 as shown in the attached drawing I give 0V at pin "1" and 24V at pin "2" change the part number of the motor in program and change the parameter P1215 to 1 and calibrate the motor to home position but when I try to jog it, it didn't release the brake. I really need help on this. AttachmentS110 brake (2).pdf (234 Downloads) |
Follow us on