12/17/2019 7:34 PM | |
Joined: 3/28/2015 Last visit: 3/24/2023 Posts: 703 Rating:
|
Hello, Perhaps the following manual might help: SINUMERIK 828D SINAMICS S120 Parameter description P0971: Save drive object parameters / Drv_obj par save Setting to save the parameter of the particular drive object in the non-volatile memory. When saving, only the adjustable parameters intended to be saved are taken into account. Value: 1: Save drive object P0977: Save all parameters / Save all par Saves all parameters of the drive system to the non-volatile memory. When saving, only the adjustable parameters intended to be saved are taken into account. Value: 1: Save in non-volatile memory - downloaded at POWER ON |
Last edited by: Jen_Moderator at: 12/18/2019 09:50:19Optimized link. Eng.Mohamed Ibrahim |
|
12/17/2019 8:59 PM | |
Joined: 3/28/2015 Last visit: 3/24/2023 Posts: 703 Rating:
|
Hello, Perhaps the attached manual might help: SINAMICS S120 Function Manual Drive Functions Saving parameters in a non-volatile memory : The modified parameter values are stored in the volatile RAM. When the drive system is switched off, this data is lost. The data must be saved retentively on the memory card, so that it is available the next time the drive is switched on. ● Save parameters - device and all drives p0977 = 1; automatically reset to 0 ● Save the parameters with STARTER
See "Copy RAM to ROM" function |
Last edited by: Jen_Moderator at: 12/18/2019 09:54:04Optimized link. Eng.Mohamed Ibrahim |
|
Follow us on