1/27/2018 8:17 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating: (879) |
Hello, Please visit below link, where you will find the application notes of torque control. Sinamics S120 - S7-1500 application notes. HTH |
2/8/2018 9:14 AM | |
Joined: 7/30/2012 Last visit: 12/21/2024 Posts: 335 Rating: (12) |
Hello.... I Haven't Find Any Examples Related To Torque Control From Above Link Can You Tell Me Which Application Example ? |
2/8/2018 9:23 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating: (879) |
SIMATIC Winder and Tension Control SINAMICS S: DCC Line Tension Control
|
Last edited by: Jen_Moderator at: 2/8/2018 10:26:10 AMOptimized links. |
|
This contribution was helpful to1 thankful Users |
2/8/2018 9:38 AM | |
Joined: 7/30/2012 Last visit: 12/21/2024 Posts: 335 Rating: (12) |
Hello!!! Thanks For Your Reply I Have Seen That Examples But In That Control Modes Are Speed Control With Encoder (P1300=21) So I'm Bit Confused I Heve To P1300=21 Or 23 ? And Its All About Stranded Library Function ? My Application Very Simple I Will Torque Set-point In Nm...Once Drive Reaches Torque Set-point It Should Stop
|
2/8/2018 11:24 AM | |
Joined: 7/30/2012 Last visit: 12/21/2024 Posts: 335 Rating: (12) |
Hello!!! Thanks For Your Reply I Need To Set P1300=23 Means , The Links Given Is Not Suitable For Me |
2/8/2018 12:47 PM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating: (879) |
Hello, You need to go with Technology Controller function with Sinamics configuration or in case of with PLC you need to change PLC CPU with technology function, so as to achieve your application. HTH. AttachmentSinamics S120 Technology function - Tension control.pdf (856 Downloads) |
Last edited by: PISCEAN 2010 at: 2/8/2018 12:49:33 PM |
|
Follow us on