9/29/2022 8:17 AM | |
Joined: 3/23/2022 Last visit: 5/2/2024 Posts: 9 Rating: (0) |
I have one more question, could you guys please advise. In Sinamic S120 manual, i saw this introduce but i dont know why need to generate a DC voltage to power the Motor Modules. At first we have AC voltage then we use Line Modules to generate DC voltage then we use Motor Modules to convert to AC voltage. It is so complicate, right? Why dont use the AC voltage to control Motor Modules. Could you please advise? ------------------------------------------------------------------------------------------ |
Last edited by: nothink at: 09/29/2022 08:19:59Last edited by: Jen_Moderator at: 09/29/2022 08:28:51New subject after splitting |
|
9/29/2022 9:07 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, I will try to answer in simple way. In case of AC induction motors, motor speed is varied by varing V/F i.e. voltage to frequency ratio. This V/F ratio variation is achieved by latest IGBTs power device modules with PMW (pulse width modulation) technology. To achieve this function, first input AC supply is rectified to DC voltage (converter) & then this DC voltage is converted to AC supply (inverter) of course variable voltage with variable frequency. This way AC induction motors speed change is achieved. In Sinamics or Siemens drives, AC power module which converts AC supply to DC is called as INFEED modules & modules which converts DC supply to AC (variable voltage variable frequency) are called as LT Power modules or Motor modules. For more information you may refer below manuals or you can search with Google. Variable frequency drives - Drive technology topics - GlobalSINAMICS Electric Drives | Drive Technology | Siemens USA |
Last edited by: PISCEAN 2010 at: 09/29/2022 09:08:08Last edited by: Jen_Moderator at: 09/29/2022 12:03:53Link optimized. |
|
This contribution was helpful to1 thankful Users |
9/30/2022 12:43 AM | |
Joined: 3/23/2022 Last visit: 5/2/2024 Posts: 9 Rating: (0) |
thank you guys so much. |
Last edited by: nothink at: 09/30/2022 00:43:46 |
|
Follow us on