12/11/2019 7:40 PM | |
Joined: 3/8/2017 Last visit: 12/11/2022 Posts: 13 Rating:
|
Hello Expert! I have urgent problem. As I asked before I'm using S1200_comb_S210. Motor article is 1FK2103-2AG10-1MA0. Yesterday there was power blackout at the factory. And then motor lose its reference position. But this is absolute motor.It should never lose although power blackout. S1200 comb S210 can be problem? should only configure with S1500 when use S210? I want to attach my TIA project but it's too large to upload. Can you tell me what is the problem? Please let me know the reason. Best regards.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/12/2019 11:32:01New subject after splitting |
|
12/12/2019 1:14 PM | |
Joined: 2/7/2018 Last visit: 2/7/2023 Posts: 177 Rating:
|
Hi, When you using an absolute encoder and perform an “absolute encoder adjustment”, the actual position will be saved within the technology object. The “absolute encoder adjustment” should be performed with the “MC_Home” function in “Mode = 7”. Have you done that? Details can be found in the motion control manual S7-1200 (Chapter MC_Home): https://support.industry.siemens.com/cs/ww/en/view/109773400 Best Regards, |
12/13/2019 12:34 AM | |
Joined: 3/8/2017 Last visit: 12/11/2022 Posts: 13 Rating:
|
Hello. Expert! Definitely I did it. But I found difference between TO_PosAx version and CPU version at the Overview of version what you attached manual. My CPU version is V4.2 but TO's one is V5.0. I have to use V6.0? It has different Encoder connection and there is selection box about Automatic transfer of encoder parameters in the device. It can be reason? I attached about version what I use CPU, S210, TO_PosAx. Give me advice. Thanks a lot.
|
Last edited by: JHPA at: 12/13/2019 00:35:31Last edited by: JHPA at: 12/13/2019 00:37:33 |
|
Follow us on