6/2/2009 10:28 AM | |
Posts: 25 Rating:
|
Hello I need to make a communication between S5 115 CP535 and S7 315 2-DP CP343-1 useing ISO communication. At the moment i have tryed useing AG_Send and AG_Receive in the S7 and Send Receive in the S5 (FB244 and FB245). I have setup the CP535 card to SEND and RECEIVE. Does anyone know if i has to use FETCH in the CP535 so i can make the connection "active" and not only passive. If anyone knows where i can find a describtion about this connection i would be very pleased. I have used the intruction on http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=22590581&load=treecontent&lang=en&siteid=cseus&aktprim=0&objaction=csview&extranet=standard&viewreg=WW regards MPE |
6/2/2009 9:47 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, The link you have specified is for Simatic TI and not Simatic S5. The correct link is here: http://support.automation.siemens.com/WW/view/en/22792412 This entry describes a send/receive connection. If you want to use Fetch, Fetch means that the S5 comes actively read dat in S7. Where write meansthat the S5 writes in the S7. But you must configure connections accordinly in the S7 and S5 as well. |
Best regards |
|
Follow us on