6/7/2017 6:02 PM | |
Posts: 2 Rating: (0) |
Hi, I'm kind a new to Siemens protocol, trying to make sure what I understood is correct about S5 that it supports 3964R protocol for data communication, is that correct? and 3964R protocol is also supported by S7 PLC as well? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/9/2017 4:14:18 PMNew subject after splitting |
|
6/7/2017 6:49 PM | |
Joined: 9/27/2006 Last visit: 5/19/2024 Posts: 12257 Rating: (2668) |
Hello asad; You are correct. A S5 PLC supports the 3964R proedure with a serial communication processor such as the CP 544. And the CP 340 (and CP 341) support the same protocol with S7-300 CPUs: Hope this helps, Daniel Chartier |
Follow us on