11/6/2009 12:53 PM | |
Joined: 10/7/2005 Last visit: 4/28/2024 Posts: 3004 Rating: (1046)
|
Hello venkatesh The "DO" command is used for indirect addressing in S5 and there areof course replacements available forit in S7. Attached is an explanation onhow the DO command works together with examples (courtesy of the S5 115 and 135 programming manuals who explain the DO command better than the 95U manual). Once you "digested" that have a look at the link below to seehow it can be done in Step7: What is the difference between STEP 7 and STEP 5 with regard to the operations for indirect addressing? Last but not least, the "DO=" command must not be confused with the "DO" command. "DO=" is a simple Block call commandand not related to indirect addressing. I hope this helps and good luck with your conversion |
Cheers |
|
Follow us on