11/18/2017 6:58 PM | |
Posts: 2 Rating: (1) |
DEAR ALL. I AM USING THE S7 1200 1214C 1BE30-0XB0. WHEN I ENERGIZE THE PLC, THERE IS NO PROBLEM, BUT AT THE TIME OF THE CONNECTION, THE FLASHING BEGINS ON THE 3 LEDS AND IT DOES NOT ALLOW ME TO CONNECT. I HOPE YOU CAN HELP ME ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/20/2017 12:42:09 PMNew subject after splitting |
|
This contribution was helpful to1 thankful Users |
11/20/2017 1:37 PM | |
Joined: 7/9/2015 Last visit: 9/25/2024 Posts: 3945 Rating: (586) |
Hi, try to do a Firmware Update and / or do a factory reset. Operating system updates for CPU 1214C, COMPACT CPU, AC/DC/RelayRegards, Towome |
|
|
This contribution was helpful to2 thankful Users |
11/22/2017 1:33 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by rick.fronda11 is split to a separate thread with the subject Simulate program in software without downloading it to plc s7 1200. Best regards |
This contribution was helpful to1 thankful Users |
12/8/2017 8:57 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by vikbar is split to a separate thread with the subject How can add 5 to 5 and so with any number that enters in hmi in tia portal?. Best regards |
Follow us on