11/4/2021 8:27 PM | |
Joined: 2/17/2020 Last visit: 9/19/2024 Posts: 1061 Rating: (192) |
Hi adamlahadi, If you buy this CPU now, you may get it with the latest released firmware version (V4.5). For the dependency on the software and firmware version, I recommend you check the following link. As you will be able to see, the firmware version V4.5 is only configurable in TIA V17. However, if you have a lower version of TIA, you should be able to configure the maximum firmware version selectable and download the project to the CPU with this version. The only thing that will appear is a warning that there are online/offline differences. |
A rating will be well appreciated. |
|
Follow us on