12/12/2022 6:37 PM | |
Joined: 10/5/2016 Last visit: 4/9/2024 Posts: 24 Rating: (2) |
And it is possible to download this program with TIA V15.1 ? Or i have to use TIA V17 ? Thank You |
12/13/2022 4:38 AM | |
Joined: 3/30/2020 Last visit: 4/26/2024 Posts: 4455 Rating: (931)
|
The short answer: The longer answer: Step7 will complain when downloading. This is only a warning and can be safely ignored. Do note that Step7 will regularly complain that the hardware configuration and hardware does not have the same firmware. The CPU will however work as the firmware version specified in the software without problems. As a bonus hint: The S7-1200 firmware V4.3 was not shipped with the software. A hardware service pack needs to be loaded. ..and No, that is the latest S7-1200 firmware that Step7 V15.1 will configure. You will have to get at least Step7 V17, if the constant warning message causes problems for you with your customer. Note that V18 has been released, though partially. See which licensing types are available for your area and buy V18. You can still decide to use the stable V17 even if you have a V18 license. Are things clear now? |
Last edited by: qwazee at: 12/13/2022 04:40:36Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on