8/24/2013 1:12 PM | |
Joined: 1/29/2006 Last visit: 5/7/2024 Posts: 446 Rating: (64) |
Hello to all! Did anybody allready try to import symbols to OPC server (Simatic Net; OPC server is configurted for S7-1200)? I am not able to do it. (see attachment!). Ihave created a symbol list with symbol editor and then exported as *.csv file and try to import it to OPC server. Format of csv filelooks OK, but whenI try to import it, nothing happens. Actually, there is a short pop-up window on screen, when I try to import, but it isshown only for a very short time, and I can not read, what it says! OPC server is working OK, I can connect my S7-1200 to WinCC V7 (through OPC), but I would like to ease WinCC configuring of OPC tags. I expected, that if I could pass symbols from S7 to OPC server, that I could see those symbols then also in OPC client application, when browsing server... . Or am I expecting too much? Every hint would be highy appretiated! Sincerely yours! uel123. AttachmentOPC SYMBOLS IMPORT.pdf (463 Downloads) |
8/26/2013 4:09 PM | |
Joined: 1/29/2006 Last visit: 5/7/2024 Posts: 446 Rating: (64) |
Hello, Rated X, thank you very much for your answer. - I created a csv file with "Symbol Editor" program, which is a part of Simatic Net installation. (at least, I think so), see attachment. - I have DB declaired in Standard mode. my OPC application (connection to WinCC SCADA V7) isbasically working, if I define tags in WinCC by myself (classic procedure,...). I am looking for a faster way of creating tags on SCADA. I do not know, how to "activate OPC symbols and browse the PLC" in mentioned dialogue? Sincerely yours! uel123. AttachmentSymbol editor.pdf (318 Downloads) |
Follow us on