10/1/2021 12:20 PM | |
Joined: 8/4/2021 Last visit: 1/18/2023 Posts: 7 Rating:
|
Hello, Stanislav thank you for your sample, It is working... Ive got CPU 1200 1214C DCDCRLY.. But the problem is, that it is working only for IO moduls on the right side of CPU, We use also GPRS and MOD BUS RTU moduls which are on the left side of SPU and with them I can not accomplish the functionality... im still stucked in the STOP mode a can not acces RUN if Im doing eny change with left side of the CPU... DO u have any Idea why is it so ??? Thank u very much... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/01/2021 13:20:00New subject after splitting |
|
10/1/2021 1:20 PM | |
Joined: 6/19/2017 Last visit: 3/21/2023 Posts: 6683 Rating:
|
Closed cause question posted twice. The second thread with the subject Need help with Option handling is published within the conference SIMATIC S7-1200. Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on