Industry Online Support
Technical Forum
11/17/2011 9:07 AM | |
Posts: 6 Rating: (0) |
Hi, I have problem with hardware configuration of Danfoss FC300. When I download hardware config, there is an error message "hardware component removed or missing HWID =287". I have set same IP adress in HW config and in FC300, same subnet mask and etc. I'm using S7 1214C and TIA v11. When I download HW config without Fc300 there is no problem. I've attached some screens of the problem. I'll be very grateful for any help. Attachmentscreens.zip (105 Downloads) |
11/17/2011 11:39 AM | |
Posts: 6 Rating: (0) |
yes, but still didn't work. |
Last edited by: small1978 at: 11/17/2011 11:40 AM |
|
11/17/2011 3:10 PM | |
Posts: 6 Rating: (0) |
unfortunately the status of FC 300 is not connected. I'll attach the text file later |
Follow us on