11/22/2013 8:22 AM | |
Joined: 10/26/2012 Last visit: 9/2/2024 Posts: 10 Rating: (1) |
Hi I have some questions about S7-1500 connectionsresources References:SIMATIC S7-1500, ET 200MP, ET 200SP Communicationhttp://support.automation.siemens.com/WW/view/en/59192925 Mentioned in this manual “for example a Basic Panel requires up to 2 connection resources for an HMI connection whereas a Comfort Panel requires up to 3 connection resources on the CPU.” But when I was in configuration Comfort communication, only occupies 2 connection resources, What configuration requires 3 connection resources? How to calculate the S7-1500 maximum connections resources HMI devices? for example CPU 1513-1 PN PM Number of connections • Number of connections, max. 128 • Number of connections reserved for ES/HMI/Web 10 • Number of connections via integrated interfaces 88 connecting to max. 29 Comfort Panels ?? PM has described the data? thanks! |
Last edited by: azimao at: 11/22/2013 8:59 AMLast edited by: azimao at: 11/22/2013 8:34 AM |
|
11/25/2013 3:04 AM | |
Joined: 10/26/2012 Last visit: 9/2/2024 Posts: 10 Rating: (1) |
Thank you for your reply |
11/27/2013 7:52 PM | |
Joined: 9/23/2005 Last visit: 8/27/2024 Posts: 4347 Rating: (1442)
|
You are wellcome :) |
Denilson Pegaia |
|
9/29/2015 10:42 AM | |
Joined: 10/4/2013 Last visit: 9/4/2024 Posts: 3 Rating: (0) |
Hope the attached file helps for the question ;) |
This contribution was helpful to3 thankful Users |
Follow us on