5/26/2022 6:07 PM | |
Joined: 8/10/2016 Last visit: 6/17/2024 Posts: 14 Rating:
|
Came across this discussion looking for what sounds like a very similar problem on one of my S7-1500F's. Did a cold start on the CPU after some work on a remote panel ET200SP (unsure if this is related in any way). CPU was stuck in a "connecting" state as previously described. The other modules in the rack appeared to be going through some sort of loop. The power/diag lights would flash then come on as if it were booting, all IO lights would come on, then after a few moments all of the IO/power/diag lights would turn off then start over. No alarms/diag text on the CPU. As I was standing there googling, it managed to get in to run mode by itself after maybe 5 min and is running now. No idea what it was stuck on. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/27/2022 08:51:33New subject after splitting |
|
5/27/2022 2:04 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi dnaines, did you have a look online on the PLC? can you share the diagnosic buffer? you can export it as textfile with the "save as.." button. If the PLC has a kind of missfunction, it is recommented to update the FW of the device. S7-1500 FW-updates can be found here: Firmware update S7-1500 CPUs incl. Displays and ET 200 CPUs (ET 200SP, ET 200pro)hope this helps, regards, |
FCK WAR! |
|
Follow us on