10/21/2015 5:31 PM | |
Posts: 288 Rating: (4) |
hello dear friends. i have a project as below: i need to measure temperature of 20 points in different positions. maximum lenght of sensors to plc is 50 meters. The plc is s7200 but i don't know if it is possible to use pt100 sensor in this distance or not. please let me know if you have another solution. best regards. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/22/2015 11:01:55 AMNew subject after splitting |
|
10/21/2015 5:52 PM | |
Joined: 12/18/2014 Last visit: 5/4/2024 Posts: 32954 Rating: (4073) |
According to the manual up to 100 m.
Attachments7200_system_manual_en-US.pdf (460 Downloads) |
This contribution was helpful to1 thankful Users |
10/21/2015 5:54 PM | |
Posts: 8946 Rating: (999) |
It is possible. |
This contribution was helpful to1 thankful Users |
Follow us on