5/28/2011 5:14 PM | |
Joined: 4/24/2006 Last visit: 5/3/2024 Posts: 8632 Rating: (1148) |
Hello, Have a look at the following links: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=6ES7314-6CG03-0AB0&caller=view https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=6ES7314-1AE04-0AB0&caller=view The 6ES7 314-6CG03 could be used as spare part, but it has onboard I/O and Profibus port. Best regards, Wizard |
5/28/2011 5:23 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Take a look for CPUs info at Technica/Cax Data tab: 6ES7314-6CG03-0AB0 6ES7314-1AE04-0AB0 6ES7314-1AG13-0AB0
So, defect one could be replaced with 6ES7314-6CG03-0AB0 for sure. With the other one depends of your project. BTW why do you think the CPU is defect? Could be the MMC is... best regards, Hristo Mihalev |
5/28/2011 5:33 PM | |
Joined: 5/28/2009 Last visit: 4/26/2024 Posts: 127 Rating: (10) |
Hi......isurya CPU314 with P/N : 314-1AG13-0AB0 this cpu is a new version V2 but6ES7314-1AE04-0AB0 this cpu olde version V1 . This two CPU's only problem in Version. The 6ES7 314-6CG03 could be used as spare part, but it has onboard I/O and Profibus port. |
Regards, |
|
5/28/2011 6:33 PM | |
Posts: 107 Rating: (0) |
HI Umencho Yes, the CPU get drip water from the pipe leakage then go thtough inside the desk panel that has this cpu indra |
5/28/2011 6:43 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
OK, In case of water or fire, fully agree to change it. best regards, Hristo Mihalev |
5/28/2011 7:19 PM | |
Posts: 947 Rating: (45) |
Maybe should use 6ES7314-1AG14-0AB0. 6ES7314-6CG03-0AB0 - is compact family CPU.He has great size, and may not fit in place of the faulty. |
5/28/2011 7:34 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
1AG14 isn't mentioned above. But this would be the perfect substitution there.
best regards, Hristo Mihalev |
Follow us on