Industry Online Support
Technical Forum
10/22/2009 11:34 PM | |
Joined: 5/28/2008 Last visit: 6/9/2024 Posts: 4509 Rating: (837) |
Dear mohit, For connecting CPU to PG we have the following possibilites: 1. Using the profibus/MPI port of the PG: You should have profibus cable with suitable length and two bus connectors: 2. Using USB port of the PG: You have to use USB PC adapter. Another old method is to use PC adapter with serial interface and connect its serial side to the Com port of a PC/PG. It's not allowed to connect SUB-D 9 pin sockets directlly between PC/PG and CPU. It won't work and may damage your com port of PC/PG as there is 24VDC on a pin of the nine pins of MPI /DP port of the CPU. Regards, |
Ayman Elotaify |
|
10/25/2009 11:39 AM | |
Posts: 37 Rating: (2) |
i think you need to check the interface by " Set PG/PC interface. |
10/28/2009 11:30 AM | |
Posts: 89 Rating: (1) |
Please tell me how to enter for MPI settings |
10/28/2009 11:35 AM | |
Posts: 89 Rating: (1) |
I have a MPI/DP port in my field PG and suggest me which Connector shoud i purchase for S7 300 |
10/28/2009 11:36 AM | |
Posts: 89 Rating: (1) |
S7 300 CPU is 317F-2DP |
10/29/2009 4:19 AM | |
Posts: 382 Rating: (47) |
Dear mohit, To add on to J_Bell input, if you are using PC Com port you cancommunicate using the following methods [see attach]. There are two setup depending which type of programming cable you have, one is 9-pin com adapter and the otheris USB adapter. Hope these information are useful toyou! with regards, how come? AttachmentTo Mohit.zip (123 Downloads) |
Last edited by: how come? at: 10/29/2009 4:29 AM |
|
Follow us on