12/21/2009 3:57 PM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hi OLAMIX, Please tell me which Module you are (MLFB No.) using for the your project, please Checked the wiring on the Output module Flape, or Here is the link fo the S7-300 Module Data http://support.automation.siemens.com/WW/view/en/8859629 & also tell me which type of Bulb or Indicating Lampyou connected on Output Side. is it 24 VDC type Or 110/220 VAC. |
Ammy |
|
12/21/2009 10:42 PM | |
Posts: 7 Rating: (0) |
ist attachement |
12/21/2009 10:44 PM | |
Posts: 7 Rating: (0) |
2nd attachement i actually made the 2nd offline, but when on line the staus is showin Run but for the outputs no valuse can be seen warm regard |
Follow us on