7/30/2011 6:13 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, Using S7-1200 with firmware V2, and Portal V11. The S7-1200 can be IO controller of an ET200M on Profinet IO. By adding a communication processor Profibus Master the S7-1200 can be a Master of a ET200M slave on profibus. See an example added as screenshot from Portal. In these IO device/Profibus slave you can use certain types of S7-300 modules SM321, SM322, ... For the excat types/versions supported see portal V11 and this FAQ. http://support.automation.siemens.com/WW/view/en/50029532 AttachmentS7-1200 and ET200M.pdf (630 Downloads) |
Last edited by: jklm at: 7/30/2011 6:15 PMBest regards |
|
This contribution was helpful to
1 thankful Users |
8/20/2015 11:16 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4837 Rating:
|
New question published by ugpromavt is split to a separate thread with the subject Connect s7-1214c and IM153-4, not go to run. Best regards |
6/20/2016 5:57 PM | |
Posts: 4 Rating:
|
i have CPU S7 1200 and i want to use some modules that are family of s7300 is that possible??? |
Last edited by: jamal ouza at: 6/20/2016 6:11:27 PM |
|
6/20/2016 6:17 PM | |
Joined: 9/27/2006 Last visit: 2/7/2023 Posts: 11951 Rating:
|
Hello jamal; Our friend jklm already answered the question you ask very clearly, in his original reply (2011).. See the posts above. S7-300 modules are not compatible physically with S7-1200 CPUs. But they can be connected to a S7-1200 CPU as part of a ET 200M slave, either over Profibus (using a IM 153-2 head module) or over Profinet (using a IM 153-4 head module). Have a look at this presentation of ET 200M systems, on Siemens electronic catalog pages: http://w3.siemens.com/mcms/distributed-io/en/ip20-systems/et200m/Pages/Default.aspx Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 6/20/2016 6:17:37 PM |
|
6/21/2016 11:49 AM | |
Posts: 4 Rating:
|
I want to use any s7 300 modules is that possible |
6/21/2016 2:20 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4837 Rating:
|
New question published by jamal ouza is split to a separate thread with the subject Where I can download step 7 pro. Best regards |
Follow us on