10/28/2018 8:27 AM | |
Joined: 11/15/2015 Last visit: 1/31/2025 Posts: 179 Rating:
|
Hello JORDAN007, Have a look at this link https://support.industry.siemens.com/tf/us/en/posts/connecting-cp343-1-lean-to-wincc-runtime-advanced/201169/?page=0&pageSize=10 Regards ========================================================= Look for alternative not for the correct answer.... |
Look for alternative not for the correct answer...if this is helping you rate it. |
|
10/28/2018 10:39 PM | |
Posts: 16 Rating:
|
|
10/29/2018 6:47 AM | |
Joined: 11/15/2015 Last visit: 1/31/2025 Posts: 179 Rating:
|
Hello, Have a look at this link https://support.industry.siemens.com/cs/ww/en/view/87054082 Regards, ========================================================= Look for alternative not for the correct answer.... |
Last edited by: Jen_Moderator at: 10/29/2018 10:43:03 AMOptimized link. Look for alternative not for the correct answer...if this is helping you rate it. |
|
11/2/2018 1:46 PM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello JORDAN007 you do not need any special Hardware or software. If you have PLC and WinCC Advanced in the same Project then its no problem because if you do the connections correct then everything will run automatically (you only have ot set the PPGPC Settings on the Runtime System) If you have th PLC in a Classic Project and the Advanced RT in TIA then use this for avoiding Problems: https://support.industry.siemens.com/cs/de/en/view/73502293 If you want to use a manualy created HMI Connection then be sure that you use the IP Adress of the CP and the Slot Number Of The CPU on PLC side you do not have to do anything than configuring the CP343-1 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on