12/18/2015 11:12 AM | |
Joined: 4/9/2013 Last visit: 1/30/2024 Posts: 26 Rating: (0) |
Hi all, I also have a problem with my SF red LED witch is ON now. I've checked the diagnostic buffer but everything is ok there. The CPU is in RUN mode. I have compared all the offline/online blocks and the result was: "Blocks are identical". The Hardware Config is also ok.(all devices green in online mode) I'm using S7-314C and TIA Portal V13 SP1. What can be the problem? ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 12/18/2015 3:53:18 PMNew subject after splitting |
|
12/18/2015 4:22 PM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980) |
Hello, have you a screenschot of the Deviceview of the PLC in Online mode? Christoph |
12/20/2015 1:06 AM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
Dear Razvansql, Please update your software, update 6 is already available. Updates for STEP 7 V13 SP1 and WinCC V13 SP1 If there are no diagnostic errors in the diagnostic buffer then it might be the firmware version and/or the TAIP software. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on