8/23/2012 12:14 PM | |
Posts: 12 Rating: (0) |
Thanks for your reply dchartier, I will try both options. Seems to be working. Regards, |
8/23/2012 12:41 PM | |
Posts: 12 Rating: (0) |
Dear Umencho, Can u pls let me know how wud I expand the process image area for PQW. Regards, |
8/23/2012 12:51 PM | |
Joined: 9/27/2006 Last visit: 10/9/2024 Posts: 12285 Rating: (2685)
|
Hello P. Singhania; Have a look at the following extract from this FAQ. It might be helpful: http://support.automation.siemens.com/WW/view/en/18325417 The current size of the process image of the CPU implemented is available online via "PLC > Diagnostics/Settings > Module Status > Performance data". Depending on the type of CPU, you can also make the process image larger or smaller in the hardware configuration ("Object Properties"[CPU] > "Cycle/Clock marker"). More information on the size of the process image and on the peripheral address area is available in the following manuals:
Hope this helps, |
Follow us on