Industry Online Support
Technical Forum
9/8/2014 6:21 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306)
|
Hello YogendraG On the face of it, there should not be any issue in this. You can have One set of Redundant Profibus network from the MPI/DP Ports of both CPUs ( Configured as Profibus ) with 2 Racks connected Create a 2nd Redundant Profibus Set from the DP Ports of both CPUs - Connect the remining 2 racks with the Redundant set of modules to this network. Configure the module redundancy in the software. Still just to be sure, I think you should raise a : support request and be sure about it. Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
Follow us on