4/16/2011 7:45 AM | |
Posts: 21 Rating: (1) |
Dear All i need some help about cpu315F , icommission a new CPU 315F it is in Running mode i did some signal Test during work i found one of the Analog card have wrongconfigurationtype i made it correctand download theoriginalprogram with this HWConfig rationChanging, but this time CPUgo in stop mode ididn'tknow the password but i give 3618 this we are using mostly in our systems. Please help Best Regard Bukhari
AttachmentHot_Gas_.zip (44 Downloads) |
4/16/2011 7:55 AM | |
Posts: 1064 Rating: (72) |
Waht does the diagnostic buffer say ? Can you post it |
5/4/2011 10:30 AM | |
Posts: 21 Rating: (1) |
dear all Iget success to make compiling the sftey program. BUT After download the program in to cpu315F-2dp it remains STOP PLEASE HELP AttachmentHot_Gas_chang config.zip (41 Downloads) |
Last edited by: Bukhari at: 5/4/2011 10:34 AM |
|
5/4/2011 10:34 AM | |
Posts: 21 Rating: (1) |
HERE I ALSO ATTACEHED THE DIAGNOSTI BUFFER AttachmentDiagnose4-5-11.zip (37 Downloads) |
5/4/2011 11:11 AM | |
Joined: 10/7/2005 Last visit: 5/2/2024 Posts: 3004 Rating: (1046)
|
Hello Bukhari not too sure how you managed to compile the Safety program without errors, I still get errors and there's also write access to the F-DB'sfrom the standard program. As far as I''m concernend, I wouldn't trust the integrity of your modified S7 program (which seems based on an online backup). Theonly meanignful advise I can offer is again(see also THIS thread) tofirstly get hold of a useable offline backup of the original S7 project. |
Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on