Industry Online Support
Technical Forum
5/11/2010 1:31 PM | |
Joined: 4/24/2006 Last visit: 10/18/2024 Posts: 8746 Rating: (1169) |
Dear LPAR, Have a look at this link: how do you use WinCC flexible to transfer a project to an operator panel via S7-routing? You should have WinCC flexible 2008, but it is not possible with panel TP177A. See notes nr. 4 Best regards, Wizard |
Last edited by: Wizard at: 5/11/2010 3:03 PM |
|
5/11/2010 3:14 PM | |
Joined: 4/24/2006 Last visit: 10/18/2024 Posts: 8746 Rating: (1169) |
Dear LPAR, I have no possibility to test anything So the fastest is to ask Siemens Hotline: SupportRequest Please let us know the answer. Best regards, Wizard |
This contribution was helpful to1 thankful Users |
5/17/2010 10:54 AM | |
Posts: 28 Rating: (0) |
Did some mailing with Siemens and came up with this: I explaned the question and refered to this forum. They give me the link i also got here. (http://support.automation.siemens.com/WW/view/en/32235096) I explaned that the option to download via routing is also available with a TP177A, with a screenshot. They say that the basic panels, like the TP177A,are limited in funtionallities. And with the link they send it is clear that the routing will not work. First point is that the TP177B has it. That's also a basic panel. Second is that the link isn't clear. Or the WinCC Flex 2008 is not clear. WhatI personally think, but can't test it, is that the note is made if you use the HMI as 'router'. All HMI's mentioned in the note have 2 ports. With all others routing will not work because there is simply no other port to route to. But in my situation the HMI doesn't got to have a routing option (I think) so i guess it will work. Only the PLC got to have the routing function. It's still not very clear to me. Anyone can light me? Greetings Leon |
Follow us on