3/28/2011 10:47 AM | |
Joined: 4/30/2010 Last visit: 3/17/2022 Posts: 43 Rating:
|
hi, In the application i am using cpu1212c in that high speed counter has to counts 1500pulse/sec is it possible ?
|
3/29/2011 5:52 AM | |
Joined: 4/30/2010 Last visit: 3/17/2022 Posts: 43 Rating:
|
hi i am getting the pulse upto 5000 rpm hsc is counting upto that,after that only it is going to zero |
3/29/2011 9:44 AM | |
Joined: 9/8/2009 Last visit: 1/20/2023 Posts: 1410 Rating:
|
rpm = rounds per minute, while counter counts pulses. Your explanation doesn't make any sense. |
3/30/2011 1:20 PM | |
Posts: 4 Rating:
|
The speed is 5000 rpm |
3/31/2011 6:37 AM | |
Joined: 4/30/2010 Last visit: 3/17/2022 Posts: 43 Rating:
|
hi 10pulses in one rotation |
4/6/2011 7:18 AM | |
Joined: 4/30/2010 Last visit: 3/17/2022 Posts: 43 Rating:
|
hi Single Phase up to 100kHz for i0.0 is using as hsc i/p |
Follow us on