12/20/2006 4:03 AM | |
Posts: 23 Rating: (0) |
Hi, I need help. I have read and tried the guide below but can't seem to get it to work. I have created the Read_RTC(VB0) block and load the sample TP177.hmi(Area pointer : Add VW0) file. What am I missing? Please advice. http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=19322242&caller=view AttachmentTimestamp.zip (123 Downloads) |
12/20/2006 5:37 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hi, do you know this FAQ => http://support.automation.siemens.com/WW/view/de/24122973 greetings, |
12/21/2006 2:14 AM | |
Posts: 23 Rating: (0) |
Hi Brain, Yes I know about the guide but it did state Achtung: Dieser Beitrag kann nicht bei den Bediengeräten TP170A, TP170micro und TP177micro verwendet werden. Informationen zur Uhrzeitsynchronisation zwischen einem TP170A, TP170micro bzw. TP177micro und der S7-200 mit WinCC flexible finden Sie unter Beitrags-ID: 19323674. So I refer to this one here I tried to Transfer the CPU system time to the panel but it don't seem to work for me. On the TP177Micro do I need to create a new tag for the date/time or it will sync automaticlly? Pls advice. |
Last edited by: whtrader at: 12/21/2006 2:24 AM |
|
1/31/2007 9:00 AM | |||
Posts: 23 Rating: (0) |
[quote user="The Brain"]Hi, sorry i mean theFAQ 19323674, (TP177micro). When you use the sample project, does this project does not work? I am not a "expert" for S7 200 and normaly i use a S7 300/400. Hi, Ya I tried using the sample project but it is not working. Can someone pls confirm this? |
||
2/9/2007 12:56 PM | |
Posts: 3149 Rating: (171)
|
Hi, well, I don´t have a S7-200 CPU so I cannot check this. Which WinCC flexible and which MicroWin version are you using? nemo |
2/9/2007 2:10 PM | |
Joined: 9/5/2007 Last visit: 3/7/2023 Posts: 317 Rating: (17) |
Back to basics first. Do you have comms between the cpu and the HMI? I.e. are the adresses correct, baud rate etc.? Once you know this is ok then you can start to debug the problem. I have used this FAQ test project before and it was ok. Sorry if you have already done this but try it. |
3/19/2007 3:18 AM | |
Posts: 23 Rating: (0) |
Hi skimmer, Yes there is connection between the PLC and TP177 Micro. Did you use S7-200 with the test project? I'll try the test project once more. |
3/19/2007 8:51 AM | |
Joined: 9/5/2007 Last visit: 3/7/2023 Posts: 317 Rating: (17) |
Yes I did. As far as I remember it just worked. Makes sure you double check all the basics in case you changed something. |
3/22/2007 3:32 AM | |
Posts: 23 Rating: (0) |
You were right. Finally, I got it to work. Thank you all for the help. |
Follow us on