2/24/2016 5:20 PM | |
Joined: 2/2/2016 Last visit: 2/8/2023 Posts: 221 Rating: (2) |
it is dc geared motor from Nidec 404.961 it has hall effect sensor which gives pulses.in my configuration i haven't used the feedback yet. I configured the axis technology and I used its commands, I downloaded the program to the PLC and I push start but i didn't get output from PTO. However when I configure it to PWM it gives output. the whole program is activated except the CTr_PWM and Move absolute. I neither used any limit switches in hardware nor software the attached file shows the program and axis configuration.
AttachmentDoc1.pdf (310 Downloads) |
Last edited by: engma at: 2/24/2016 5:22:56 PMLast edited by: engma at: 2/24/2016 7:08:35 PM |
|
2/24/2016 9:42 PM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
Did you try moving it manually trough the "commissioning" control? |
2/25/2016 6:45 PM | |
Joined: 2/2/2016 Last visit: 2/8/2023 Posts: 221 Rating: (2) |
I didn't connect any drive, I will use simple H-bridge to drive the dc motor. Is it obligatory to connect the drive ? it gives light with PWM without connecting any output or drive. I activated manual control but the commands weren't activated as shown in pic.
AttachmentDoc1.pdf (329 Downloads) |
Last edited by: engma at: 2/25/2016 6:48:24 PMLast edited by: engma at: 2/25/2016 6:51:15 PMLast edited by: engma at: 2/25/2016 6:57:40 PMLast edited by: engma at: 2/25/2016 7:20:22 PM |
|
2/25/2016 8:39 PM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
Take the device offline |
2/25/2016 9:30 PM | |
Joined: 2/2/2016 Last visit: 2/8/2023 Posts: 221 Rating: (2) |
ok, I will my version is v13 sp1 |
Follow us on