5/3/2017 5:18 PM | |
Posts: 2826 Rating: (685) |
Hello Jiri. Following through on the the "AT" operator idea Duris_I gave (quoted below) - see the attached UDT and FB source files. For the code to work, a UDT is created for the bit structure. The FB is also using a non-optimized DB structure where your system DB uses optimized structure. It is not a problem though. You will have to clarify why you have 16 bits in the structure. 8 called "clock" and 8 called "pulse". The code guesses on what is required. You will feed "Clock_Byte" to the input and "System_DB".ClockPulses to the output of the FB when it is called. Regards.
Update 1: AttachmentClockBitStructures.zip (116 Downloads) |
Last edited by: #dP at: 5/3/2017 5:19:54 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on