4/10/2012 4:56 PM | |
Joined: 1/30/2006 Last visit: 4/26/2024 Posts: 103 Rating: (16) |
Selami DAL, Unless this new script problem shows the same error (#429 ActiveX Component can't create object), the question should be in a new thread on this forum. That stated, would you please explain how the script is not working. Is it throwing an error when it executes? Or does it simply not operate as you expect? Does Flex even allow it to compile? I have tested the logic of the script in my MP377, and it does work as I would expect. However, I did have to modify the whitespace as you had displayed it in your post. For example, this . . . [code]If SmartTags("A")=True Then [/code]will cause a compiler error because VBScript does not like line breaks in the middle of IF...THEN statements. The correct arrangement would be [code]If SmartTags("A")=True Then [/code] This is the only problem I had in copying and pasting your script into my Flex project, but I guess that you entered it that way in this forum to make it easier to read. I have attached a PDF copy of the script as it appears in my Flex application. When you get a chance, please give more detail on how the script is not working. Very best regards, The Captive Engineer AttachmentEasyLogicScript.pdf (55 Downloads) |
Follow us on