10/7/2020 12:48 PM | |
Joined: 11/14/2013 Last visit: 10/27/2021 Posts: 11 Rating:
|
Hi I have created a script to create and write data to Excel file. Works fine with TIA V16 in simulation, but doesn't work when downloaded to TP900. Seems it doesnt like the following for example: Objectway = CreateObject("Scripting.FileSystemObject") also IF Not Objectway.FolderExists(Folderway) THEN My question is this: Is there some difference between my commands and the ones in the TP900? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/07/2020 14:07:19New subject after splitting |
|
10/7/2020 7:29 PM | |
Joined: 7/5/2013 Last visit: 8/7/2024 Posts: 3108 Rating:
|
Hello Allan, the reason is that there are Differences between the VB script functions of Windows and WinCE. When running the script on a panel you have to use
For more information check the VBScript_WinCE.pdf in the link above. Frink |
Pi is exactly three! |
|
10/19/2020 3:27 PM | |
Joined: 8/3/2009 Last visit: 8/7/2024 Posts: 13486 Rating:
|
Hello you have to use this Syntax/example: https://support.industry.siemens.com/cs/ww/en/view/59604194 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on