10/31/2011 1:41 PM | |
Posts: 3037 Rating:
|
Hello, The download does not work with any adapter. You should see the following FAQ for MPI download. How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? Tweety |
11/2/2011 8:15 PM | |
Posts: 54 Rating:
|
Yes, the resistors are correct, I am using the PC adapter from the CPU to the PC. Yesterday a made transfers but the remote control is not working. |
11/3/2011 4:54 PM | |
Posts: 3037 Rating:
|
Hello, You do a download for your project from computer to a panel. PC/MPI-Adapter is not released for download to a panel. You can see this in this FAQ: What transfer options are available in the various operator panels? See the document "Projecttransfer_V1_2_e.pdf Tweety |
11/7/2011 11:28 AM | |
Posts: 3037 Rating:
|
Hello, You can download your Step 7 project about a PC/MPI adapter. You can download your WinCC flexible project about MPI to OP77B or TP177B. You can not download your WinCC flexible project about a PC/MPI adapter. The MPI download about PC/MPI adapteris not tested and not approved for panels OP77B and TP177B. You must use the MPI download without this PC/MPI adapter. See in the manual, page 54. SIMATIC HMI WinCC flexible 2008 Communication Part 1 You can see this notice on the page 54. Notice The PC adapter is not approved for MPI transfer. |
11/9/2011 11:16 AM | |
Posts: 3037 Rating:
|
Hello, You can use the MPI transfer about a CP, for example CP 5512 or CP 5611. You can use another kind of transfer (serial). How can you transfer a WinCC flexible project serially to a panel? You need for serial transfer to OP77B a RS 232 cable. What is the serial cable assignment for transferring the configuration to a Windows-based device? You need for serial transfer to TP177B a RS 232 Multimastercable. What transfer options are available in the various operator panels? |
Follow us on