10/10/2016 9:59 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980) |
Hello, which Sofware packes you have installed and which Operation system? |
10/10/2016 10:17 AM | |
Posts: 14 Rating: (0) |
i use win 10 and i installed s7 300 |
10/10/2016 1:47 PM | |
Posts: 14 Rating: (0) |
Sorry, you mean the parts i installed when installing SIMATIC maneger or the version I'm using, I'm using s7 300 v5.5. Sorry, I'm not good at English. |
10/10/2016 5:12 PM | |
Posts: 14 Rating: (0) |
- Components - Step 7 v 5.5 sp3 - Automation License maneger v5.2 - PLC sim v5.4 - S7 PCT - Help |
10/10/2016 9:11 PM | |
Joined: 9/3/2008 Last visit: 4/25/2024 Posts: 920 Rating: (157) |
Step7 5.x is NOT compatible with Windows 10. It will not work. You will have to use the "Compatibility Tool for Automation and Drive Technology" to check what operating system is compatible with the different software you are using. For Step7 5.5 SP3 it would be Windows 7. |
Last edited by: Michael K at: 10/10/2016 9:13:34 PMMichael |
|
This contribution was helpful to1 thankful Users |
Follow us on