1/2/2017 2:44 PM | |
Joined: 7/20/2015 Last visit: 4/23/2024 Posts: 153 Rating: (27) |
Hello OMKRIS2017 Try this For SFC13 How do you read out the diagnosis data of a PROFIBUS DP slave with the SFC13 "DPNRM_DG" and how do you evaluate the data in the user program?https://www.youtube.com/watch?v=S5y_zutWsyY For SFC 51 How is a DP slave's diagnostic data read out with SFC 51 "RDSYSST" (with an integrated DP interface on the CPU as the DP master)?SANDEEP Bakoliya |
Last edited by: Sandeep Bakoliya at: 1/2/2017 3:02:41 PMIf I could help you, you can use the RATE button. Thank you. Last edited by: CS Moderator at: 1/3/2017 12:17:58 AMVideo integrated Regards |
|
This contribution was helpful to1 thankful Users |
1/3/2017 8:25 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
hi OMKRIS2017, have a look toSandeep Bakoliya´s entry above. You will find an application example in the FAQs he posted. Have a try to program it with the help you got. When you have problems and it doesn´t work, tell us specific what the problem is and what you don´t understand. Give us the information if the functions give an error and which state they have, if it doesn´t work. hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
Follow us on