10/12/2022 6:13 AM | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Joined: 12/16/2021 Last visit: 8/22/2023 Posts: 126 Rating: (1) |
Hi VJAKKANI Mention communication interface between the devices Regards
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
If The Information Helpful, Then Don't Forget Give (To thank ) and Rate It |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
10/12/2022 8:22 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Are you using MDS or replacing 11 KW DC motor by 20 Kw motor? Please try factory reset & then load new motor parameter & conduct optimisation, in case you are replacing 11 Kw motor by 20 Kw motor. |
10/13/2022 7:30 AM | |
Joined: 4/6/2021 Last visit: 9/15/2024 Posts: 21 Rating: (0) |
Sir We are replacing 11kw mtoe with 20kw Driver factory rest done 23,24,25 and 26 optimization is ok Field weakning optimization not completing. Showing optimization aborted due to internal case (409) |
10/13/2022 8:08 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Significance of 409 is speed dropped below by more than 12.5%. Please refer r50047[1] & r50047[2] values. BTW are you conducting field weakening optimization on load or without load? Please check, it should be without load. |
Follow us on