9/21/2010 10:20 PM | |
Joined: 9/27/2006 Last visit: 3/16/2025 Posts: 12344 Rating:
|
Hello Ton; Here you will find an application note describing Thin panels (TP 277/377 thin clients) and the different ways they can be used ina project. Note that the this client by definition has no internal processing power, it only acts as a display with control capabilities. Everything is done on the server, so you always depend on the server's processing power and the qualitiy of the link between server and clients. http://support.automation.siemens.com/WW/view/en/35122024 "Without additional cost"... You have enough experience with Siemens up to now to understand they offer great products, but never "without additional cost"... ;-) Hope this helps, Daniel Chartier |
This contribution was helpful to
1 thankful Users |
9/22/2010 11:27 AM | |
Joined: 4/24/2006 Last visit: 3/14/2025 Posts: 8894 Rating:
|
Dear Ton Verra, You can use the WinCC flexible option: WinCC flexible Sm@rtAccess it is a license for panel. Perhaps these links might help: http://support.automation.siemens.com/WW/view/en/19865167 http://support.automation.siemens.com/WW/view/en/18657078 Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
Follow us on