4/18/2018 3:45 PM | |
Posts: 13 Rating: (0) |
Hi, We are trying to do a small poc on IOT for that we have selected seimens devices ( ac motor,drive, BOP-2..etc). We dont have any prior knowledge on these devices.We managed to connect and power the devices.It looks good but after I commissioned the drive and tried to start motor manually from the drive it is not spinning but making noise for around 10 seconds and then beeps. I can see 2 falults always there: 1. A8526 2.A7991 .. I am not able to remove them. I really no clue why motor is not spinning. Here are the list of devices. 1 .SINAMICS G120 CONTROL UNIT CU240E-2 2. SINAMICS S120 CONVERTER POWER MODULE PM340 INPUT: 1AC 200-240V, 50/60HZ OUTPUT: 3AC 2,3A 3. MICROMASTER 4 Line reactor 200V-240V 1AC 3.4A Base FSA-9.5MH not base with V20 4.Siemens Motor 1LA7063-4AB10-Z 5.SINAMICS G120 Basic Operator Panel(BOP-2) I have attached the pics and connection diagram aswell. I stuck here please help here Thanks, Bhaskar
Attachmentconn.docx (60 Downloads) |
Last edited by: mbredd at: 4/18/2018 4:06:30 PM |
|
Follow us on